| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub SetReferenceConstellationValues( _ ByVal constellationValues() As Single _ ) | |
| C# | |
|---|---|
public virtual void SetReferenceConstellationValues( float[] constellationValues ) | |
| C++/CLI | |
|---|---|
public: virtual void SetReferenceConstellationValues( array<float>^ constellationValues ) | |
Parameters
- constellationValues
- The reference I/Q constellation values to use
Order of array is
[ real{S(1,1)}, imag{S(1,1)}, real{S(2,1)}, imag{S(2,1)}, ...] where S(k,n) is the complex value for subcarrier k in OFDM symbol n; subcarrier k is the inner (fastest-varying) index and OFDM symbol n the outer index. For multi-stream signals the per-stream blocks are concatenated stream-major: the complete subcarrier-by-symbol block for stream 0 comes first, then the complete block for stream 1, and so on. Every per-stream block has the same length, and a single-stream signal contains exactly one block.Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00