| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub SetReferenceDataValues( _ ByVal value() As Single _ ) | |
| C++/CLI | |
|---|---|
public: virtual void SetReferenceDataValues( array<float>^ value ) | |
Parameters
- value
- The array of reference data values (as IQ values).
This is an array of values that indicate reference data (refData) in-phase/quadrature (IQ) values. Each reference data (refData) in-phase/quadrature (IQ) value of the subcarrier is represented by a complex in-phase/quadrature (IQ) value, real part first, then imaginary part.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00