| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub SetResourceTypePerAllocation( _ ByVal ParamArray value() As Integer _ ) | |
| C++/CLI | |
|---|---|
public: virtual void SetResourceTypePerAllocation( ... array<int>^ value ) | |
Parameters
- value
- The array of resource subcarrier types associated with each allocation ID.
This property is an array of values, with one value for each allocation ID, as listed in the resource map array. The values are unitless. The valid range of resource type values are 0 = Data, 1 = Pilot, 2 = Unknown Pilot, 3 = Preamble, 4 = Idle, 5 = Unspecified, 6 = Known Data. If this array is shorter than the highest allocation ID, any values past the end are assumed to be 0.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00