Keysight 89600 VSA .NET API
SetUserIdPerAllocation Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : SetUserIdPerAllocation Method


value
The array of user IDs associated with each allocation ID.

Glossary Item Box

Sets an array of user IDs associated with each allocation ID, as listed in the resource map.

Syntax

Visual Basic (Declaration) 
Public Overridable Sub SetUserIdPerAllocation( _
   ByVal ParamArray value() As Integer _
) 
C# 
public virtual void SetUserIdPerAllocation( 
   params int[] value
)
C++/CLI 
public:
virtual void SetUserIdPerAllocation( 
   ... array<int>^ value
) 

Parameters

value
The array of user IDs associated with each allocation ID.

Remarks

This property is an array of values, with one value for each allocation ID, as listed in the resource map array. The values are unitless. The user ID value is used to determine the DataBurstInfo "per User" result mapping associated with each allocation. If this array is shorter than the highest allocation ID, any values past the end are assumed to be 0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also