Keysight 89600 VSA .NET API
SymbolPhaseCompensationFrequency Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : SymbolPhaseCompensationFrequency Property


Glossary Item Box

Gets or sets the frequency in hertz used for symbol phase compensation of the signal under test.

Syntax

Visual Basic (Declaration) 
Public Overridable Property SymbolPhaseCompensationFrequency As Double
C# 
public virtual double SymbolPhaseCompensationFrequency {get; set;}
C++/CLI 
public:
virtual property double SymbolPhaseCompensationFrequency {
   double get();
   void set (    double value);
}

Property Value

The default value is 1.0e9.

Remarks

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.40

See Also