Keysight 89600 VSA .NET API
SynchronizationSearchInterval Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : SynchronizationSearchInterval Property


Glossary Item Box

Gets or sets the search interval for synchronization (in symbols).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SynchronizationSearchInterval As Integer
C# 
public abstract int SynchronizationSearchInterval {get; set;}
C++/CLI 
public:
abstract property int SynchronizationSearchInterval {
   int get();
   void set (    int value);
}

Property Value

The default value is 10 symbols.

Remarks

This property can be used with SynchronizationSearchOffset to reduce the search region for synchronization, which can speed up measurement processing, or provide more robustness for certain measurements.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.0

See Also