| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property TransmitterAntennas As Integer | |
| C# | |
|---|---|
public abstract int TransmitterAntennas {get; set;} | |
Property Value
The value is limited to the number of Agilent.SA.Vsa.Input.MeasurementChannels defined in the Input configuration. When CrossCorrelatedEvmEnabled = true, the limit is half the number of channels.When greater than one, MIMO analysis is enabled.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)