| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property UserBoostLevels As Single() | |
| C# | |
|---|---|
public abstract float[] UserBoostLevels {get; set;} | |
| C++/CLI | |
|---|---|
public: abstract property array<float>^ UserBoostLevels { array<float>^ get(); void set ( array<float>^ value); } | |
Property Value
The default value is an array of length 1, with the value equal to 1.This property is an array of values, with one value for each user ID in the resource map array. The values are unitless. A value of 1 means no power boosting, while a value of 2 means there is a 6.02 dB power boost for the user ID. If this array is shorter than the highest user ID, any values past the end are assumed to be 1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)