Keysight 89600 VSA .NET API
MultipleAccessScheme Enumeration
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : MultipleAccessScheme Enumeration


Glossary Item Box

The multiple access scheme used in the signal to be analyzed.

Syntax

Visual Basic (Declaration) 
Public Enum MultipleAccessScheme 
   Inherits System.Enum
C# 
public enum MultipleAccessScheme : System.Enum 
C++/CLI 
public enum class MultipleAccessScheme : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
DftDFT Multiple Access.22.20
NomaNon-Orthogonal Multiple Access.—
NoneNo multiple access scheme—
ScmaSparse Code Multiple Access.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also