| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property CodeWordSize As Integer | |
| C# | |
|---|---|
public abstract int CodeWordSize {get; set;} | |
Property Value
The value must be a power of two, and is rounded up if necessary to get to a power of two. The default value is 4. The minimum is 2, and the maximum is 8.Note that this is not the size of one code word. It is the number of code words for each layer at each spreading value. The number of bits in a code word is log2(CodeWordSize).
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00