Keysight 89600 VSA .NET API
NumberOfLayers Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > ScmaSettings Class : NumberOfLayers Property


Glossary Item Box

Gets or sets the number of layers.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property NumberOfLayers As Integer
C# 
public abstract int NumberOfLayers {get; set;}
C++/CLI 
public:
abstract property int NumberOfLayers {
   int get();
   void set (    int value);
}

Property Value

The default value is 2. The minimum is 1, and the maximum is 8.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also