Gets or sets the spreading factor (number of RUs over which each symbol is spread).
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property SpreadingFactor As Integer |
| C# | |
|---|
public abstract int SpreadingFactor {get; set;} |
| C++/CLI | |
|---|
public:
abstract property int SpreadingFactor {
int get();
void set ( int value);
} |
Property Value
The default value is 2. The minimum is 1, and the maximum is 6.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 21.00
See Also