Keysight 89600 VSA .NET API
SymbolSubcarrierBlock Class Members
See Also  Properties 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : SymbolSubcarrierBlock Class

Glossary Item Box

The following tables list the members exposed by SymbolSubcarrierBlock.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorSymbolSubcarrierBlock ConstructorInitializes a new instance of the SymbolSubcarrierBlock class.  30.40
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertySubcarriersGets the array of subcarriers represented as integers.  30.40
Public PropertySymbolsGets the array of symbols represented as integers.  30.40
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also