Keysight 89600 VSA .NET API
SynchronizationMode Enumeration
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : SynchronizationMode Enumeration


Glossary Item Box

Methods used to synchronize to the signal.

Syntax

Visual Basic (Declaration) 
Public Enum SynchronizationMode 
   Inherits System.Enum
C# 
public enum SynchronizationMode : System.Enum 
C++/CLI 
public enum class SynchronizationMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
CyclicPrefixSynchronize using auto-correlation based on any cyclic prefix and/or cyclic suffix content of the signal, followed by frequency-domain correlation to a known preamble or pilot pattern.—
TimeCorrelationSynchronize using time-domain correlation to a known preamble or pilot pattern.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also