Keysight 89600 VSA .NET API
BitLoadingType Enumeration
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace : BitLoadingType Enumeration


Glossary Item Box

Specifies the modulation type of a burst

Syntax

Visual Basic (Declaration) 
Public Enum BitLoadingType 
   Inherits System.Enum
C# 
public enum BitLoadingType : System.Enum 
C++/CLI 
public enum class BitLoadingType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BpskBpsk modulation—
Qam10241024-QAM modulation—
Qam128128-QAM modulation—
Qam1616-QAM modulation—
Qam20482048-QAM modulation—
Qam256256-QAM modulation—
Qam3232-QAM modulation—
Qam40964096-QAM modulation—
Qam512512-QAM modulation—
Qam6464-QAM modulation—
Qam88-QAM modulation—
QpskQpsk modulation—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.0

See Also