Keysight 89600 VSA .NET API
EqualizerControl Enumeration
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace : EqualizerControl Enumeration


Glossary Item Box

the equalization control.

Syntax

Visual Basic (Declaration) 
Public Enum EqualizerControl 
   Inherits System.Enum
C# 
public enum EqualizerControl : System.Enum 
C++/CLI 
public enum class EqualizerControl : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FullThe equalization is fully processed.—
OffThe equalization is off.—
PartialThe equalization is partial, which means that the time domain response is limited as required by docsis upstream spec.—
UserCustom user supplied equalization using frequency domain complex coefficients—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.0

See Also