Keysight 89600 VSA .NET API
EqualizerTraining Enumeration
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace : EqualizerTraining Enumeration


Glossary Item Box

Types of subcarriers used for training the equalizer.

Syntax

Visual Basic (Declaration) 
Public Enum EqualizerTraining 
   Inherits System.Enum
C# 
public enum EqualizerTraining : System.Enum 
C++/CLI 
public enum class EqualizerTraining : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
PilotsThe equalizer is computed using Pilot subcarriers.—
PilotsAndComplementaryPilotsThe equalizer is computed using Pilot and Complementary Pilots subcarriers.—
PilotsAndComplementaryPilotsAndDataThe equalizer is computed using the Data subcarriers in addition to the Pilot and Complementary Pilots subcarriers.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.0

See Also