Keysight 89600 VSA .NET API
CenterOffset Property
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace > MeasurementExtension Class : CenterOffset Property


Glossary Item Box

Gets or sets the offset from the VSA measurement center frequency to the DOCSIS carrier center frequency.

Syntax

Visual Basic (Declaration) 
Public Overridable Property CenterOffset As Double
C# 
public virtual double CenterOffset {get; set;}
C++/CLI 
public:
virtual property double CenterOffset {
   double get();
   void set (    double value);
}

Remarks

This parameter allows you to capture and analyze just the active subcarriers instead of needing to capture the entire carrier bandwidth (102.4 MHz).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also