Keysight 89600 VSA .NET API
ExcludeBandsDefinition Property
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace > MeasurementExtension Class : ExcludeBandsDefinition Property


Glossary Item Box

Gets or sets the excluded band vector.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property ExcludeBandsDefinition As Integer()
C# 
public abstract int[] ExcludeBandsDefinition {get; set;}
C++/CLI 
public:
abstract property array<int>^ ExcludeBandsDefinition {
   array<int>^ get();
   void set (    array<int>^ value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also