Keysight 89600 VSA .NET API
IsBitErrorRateAnalysisEnabled Property
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace > MeasurementExtension Class : IsBitErrorRateAnalysisEnabled Property


Glossary Item Box

Gets or sets a value indicating whether bit/packet error rate (BER/PER) information is calculated and shown on the BER/MER Summary table.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsBitErrorRateAnalysisEnabled As Boolean
C# 
public abstract bool IsBitErrorRateAnalysisEnabled {get; set;}
C++/CLI 
public:
abstract property bool IsBitErrorRateAnalysisEnabled {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also