Keysight 89600 VSA .NET API
IsExtendedFrequencyLockRange Property
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace > MeasurementExtension Class : IsExtendedFrequencyLockRange Property


Glossary Item Box

Gets or sets a value indicating whether to enable extended frequency lock range.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsExtendedFrequencyLockRange As Boolean
C# 
public abstract bool IsExtendedFrequencyLockRange {get; set;}
C++/CLI 
public:
abstract property bool IsExtendedFrequencyLockRange {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

If false, the lock range varies depending on FftLength. If true, ExtendedFrequencyLockRangeWidth specifies the center frequency lock range for the measurement. Note that the center frequency lock range may not really be as wide as (and occasionally can be wider than) specified by ExtendedFrequencyLockRangeWidth.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also