Keysight 89600 VSA .NET API
IsNormalized Property
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace > MeasurementExtension Class : IsNormalized Property


Glossary Item Box

Gets or sets a value indicating whether to normalize IQ traces.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsNormalized As Boolean
C# 
public abstract bool IsNormalized {get; set;}
C++/CLI 
public:
abstract property bool IsNormalized {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

When true, IQ traces like IQ Meas, IQ Ref, and Error Vector are normalized so that the IQ Ref constellation points have an RMS level of one. When false, the IQ traces are not normalized, so they have units of Volts.

This parameter does not apply to MER traces.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also