Keysight 89600 VSA .NET API
IsTrackPhase Property
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace > MeasurementExtension Class : IsTrackPhase Property


Glossary Item Box

Gets or sets a value indicating whether pilot tracking tracks the average pilot phase.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsTrackPhase As Boolean
C# 
public abstract bool IsTrackPhase {get; set;}
C++/CLI 
public:
abstract property bool IsTrackPhase {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

If true, the average phase of the pilot subcarriers is tracked during pilot tracking. This means that phase variation of the pilot subcarriers is backed out of all subcarriers before they are used. This is normally needed for proper demodulation, to track frequency and phase drift in the signal.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also