Keysight 89600 VSA .NET API
PauseCount Property
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace > MeasurementExtension Class : PauseCount Property


Glossary Item Box

Gets or sets the threshold for total number of bits at which to pause the measurement.

Syntax

Visual Basic (Declaration) 
Public Overridable Property PauseCount As Double
C# 
public virtual double PauseCount {get; set;}
C++/CLI 
public:
virtual property double PauseCount {
   double get();
   void set (    double value);
}

Remarks

IsMeasurementPauseAfterCount must be set to true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.2

See Also