Gets or sets the power threshold of active or unused subcarrier auto detection
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property SubcarrierDetectionThreshold As Double |
| C# | |
|---|
public abstract double SubcarrierDetectionThreshold {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double SubcarrierDetectionThreshold {
double get();
void set ( double value);
} |
Property Value
The default value is -30dB.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also