Keysight 89600 VSA .NET API
SymbolTimeAdjustmentMode Property
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace > MeasurementExtension Class : SymbolTimeAdjustmentMode Property


Glossary Item Box

Gets or sets whether the demodulator determines the SymbolTimeAdjustment automatically.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SymbolTimeAdjustmentMode As SymbolTimeAdjustmentMode
C# 
public abstract SymbolTimeAdjustmentMode SymbolTimeAdjustmentMode {get; set;}
C++/CLI 
public:
abstract property SymbolTimeAdjustmentMode SymbolTimeAdjustmentMode {
   SymbolTimeAdjustmentMode get();
   void set (    SymbolTimeAdjustmentMode value);
}

Remarks

When SymbolTimeAdjustmentMode is set to Auto, the SymbolTimeAdjustment parameter is ignored and the demodulator attempts to choose a symbol time adjustment that maximizes MER. The actual SymbolTimeAdjustment used by the demodulator is shown in the Error Summary trace.

When SymbolTimeAdjustmentMode is set to Manual, the value specified by SymbolTimeAdjustment is used.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also