Keysight 89600 VSA .NET API
PilotPatternType Enumeration
See Also 
Agilent.SA.Vsa.DocsisUpstream.Interfaces Assembly > Agilent.SA.Vsa.DocsisUpstream Namespace : PilotPatternType Enumeration


Glossary Item Box

Specifies the pilot pattern used for a burst

Syntax

Visual Basic (Declaration) 
Public Enum PilotPatternType 
   Inherits System.Enum
C# 
public enum PilotPatternType : System.Enum 
C++/CLI 
public enum class PilotPatternType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Pattern1Pilot pattern index 1 for 2048 FFT bursts—
Pattern10Pilot pattern index 10 for 4096 FFT bursts—
Pattern11Pilot pattern index 11 for 4096 FFT bursts—
Pattern12Pilot pattern index 12 for 4096 FFT bursts—
Pattern13Pilot pattern index 13 for 4096 FFT bursts—
Pattern14Pilot pattern index 14 for 4096 FFT bursts—
Pattern2Pilot pattern index 2 for 2048 FFT bursts—
Pattern3Pilot pattern index 3 for 2048 FFT bursts—
Pattern4Pilot pattern index 4 for 2048 FFT bursts—
Pattern5Pilot pattern index 5 for 2048 FFT bursts—
Pattern6Pilot pattern index 6 for 2048 FFT bursts—
Pattern7Pilot pattern index 7 for 2048 FFT bursts—
Pattern8Pilot pattern index 8 for 4096 FFT bursts—
Pattern9Pilot pattern index 9 for 4096 FFT bursts—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.0

See Also