| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property MaxMixerLevel As Double | |
| C# | |
|---|---|
public abstract double MaxMixerLevel {get; set;} | |
This parameter applies when the ESA is used as an ADC. The ESA automatically sets its internal front-end attenuation so that the ESA first mixer maximum level does not exceed this value, given the expected Full Scale Input Range setting.
Note
If you change this value, you must close and restart the 89600 VSA software for the analyzer to recognize the change.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)