| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property OptionalFrequencyReference As Boolean | |
| C# | |
|---|---|
public virtual bool OptionalFrequencyReference {get; set;} | |
If Optional Frequency Reference (B7E) is False (default), connect the 10 MHz external reference signal directly to the 10 MHz Ref In connector near the bottom of the ESA rear panel. The close-in phase noise specs for the ESA are much better in this mode of operation. In this mode the ESA will also auto-detect the presence of the external reference signal and switch between internal and external automatically. The external reference state will be displayed in the 89600 display.
If Optional Frequency Reference (B7E) is True, you can set the external reference frequency from 1 MHz to 30 MHz. The default is 10 MHz. Connect the external reference signal to the Ext Ref In connector.Connect a short BNC cable from the 10 MHz Out connector to the 10 MHZ REF IN connector.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 14.00