Keysight 89600 VSA .NET API
SampleMode Enumeration
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.InfiniiVision Namespace : SampleMode Enumeration


Glossary Item Box

Specifies the sample rate mode.

Syntax

Visual Basic (Declaration) 
Public Enum SampleMode 
   Inherits System.Enum
C# 
public enum SampleMode : System.Enum 
C++/CLI 
public enum class SampleMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FullRateUse the full sample rate of the oscilloscope.—
UserRateUse the sample rate specified with InputExtension.UserSampleRate.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also