Keysight 89600 VSA .NET API
SampleMode Enumeration
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.Infiniium Namespace : SampleMode Enumeration


Glossary Item Box

Specifies the sample rate mode.

Syntax

Visual Basic (Declaration) 
Public Enum SampleMode 
   Inherits System.Enum
C# 
public enum SampleMode : System.Enum 
C++/CLI 
public enum class SampleMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FullRateUse the full sample rate of the oscilloscope.—
FullRateDdcUse the full rate ADC sample rate, but use hardware based DDC when possible24.20
MinimizeUse the minimum sample rate that avoids self aliasing.—
UserRateUse the sample rate specified by the user (InputExtension.UserSampleRate).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also