Keysight 89600 VSA .NET API
Agilent.SA.Vsa.HardwareExtensions.Psa Namespace
See Also  Inheritance Hierarchy
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly : Agilent.SA.Vsa.HardwareExtensions.Psa Namespace

Glossary Item Box

The Agilent.SA.Vsa.HardwareExtensions.Psa namespace contains classes and enums to control  any advanced input extension parameter for the PSA performance spectrum analyzer.  

Classes

 ClassDescription
ClassInputExtension Input Extensions for PSA instruments

Enumerations

 EnumerationDescription
EnumerationTriggerLocation Specifies the external trigger port to be used for the PSA

See Also