Keysight 89600 VSA .NET API
Signal Enumeration
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.SpectrumDemo Namespace : Signal Enumeration


Glossary Item Box

Specifies the simulated signal to use.

Syntax

Visual Basic (Declaration) 
Public Enum Signal 
   Inherits System.Enum
C# 
public enum Signal : System.Enum 
C++/CLI 
public enum class Signal : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
CachedNoiseTrigger2 In—
DefaultTrigger1 In—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also