Keysight 89600 VSA .NET API
AcquisitionType Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : AcquisitionType Enumeration


Glossary Item Box

Specifies the type of acquisitions.

Syntax

Visual Basic (Declaration) 
Public Enum AcquisitionType 
   Inherits System.Enum
C# 
public enum AcquisitionType : System.Enum 
C++/CLI 
public enum class AcquisitionType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
SequencedSpecifies Sequenced acquisition. Acquisitions from the same hardware are separate and are sequenced. All measurement acquisitions are completed before any measurement result is calculated.—
SynchronousSpecifies Synchronous acquisition. Acquisitions from the same hardware are combined. All measurement acquisitions are completed before any measurement result is calculated.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also