Keysight 89600 VSA .NET API
AnalogChannelConnection Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : AnalogChannelConnection Enumeration


Glossary Item Box

Specifies the physical input impedance and terminating circuit of the measurement hardware.

Syntax

Visual Basic (Declaration) 
Public Enum AnalogChannelConnection 
   Inherits System.Enum
C# 
public enum AnalogChannelConnection : System.Enum 
C++/CLI 
public enum class AnalogChannelConnection : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
DifferentialSpecifies a differential input (balanced termination).—
SingleEndedSpecifies a single ended input (unbalanced termination)—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also