Keysight 89600 VSA .NET API
AutoRange Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > AnalogChannel Class : AutoRange Method


Glossary Item Box

Performs a one-shot default auto-range operation on the channel.

Overload List

OverloadDescription
AutoRange()Performs a one-shot default auto-range operation on the channel.  
AutoRange(String,Int32)Performs a one-shot auto-range operation on the channel based on a criterion.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also