Gets or sets the expected ratio of the peak envelope power to average envelope power. This is defined to be 20 * log10(peak voltage / (RMS value * square root(2))). That means this value is 0 for an unmodulated CW signal. This is currently only used when the
RangeOptimization property is set to
RangeOptimization.Evm.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property EnvelopePapr As Double |
| C# | |
|---|
public virtual double EnvelopePapr {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double EnvelopePapr {
double get();
void set ( double value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 26.00
See Also