Gets or sets the noise distortion trade-off in dB to use when the
RangeOptimization is
RangeOptimization.Evm. When setting up the hardware front end for the best EVM the noise portion of the EVM will be weighted by 10^(trade-off/20) and the distortion portion weighted by 1/(10^(trade-off/20)).
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property NoiseDistortionTradeoff As Double |
| C# | |
|---|
public virtual double NoiseDistortionTradeoff {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double NoiseDistortionTradeoff {
double get();
void set ( double value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 26.00
See Also