| Visual Basic (Declaration) | |
|---|---|
Public Overloads Overrides Function Equals( _ ByVal obj As Object _ ) As Boolean | |
Parameters
- obj
- The object to compare with the current instance.
Return Value
true if the specified object has the same process id, TCP port, and whether it is a 64 bit process; otherwise, false.Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.50Reference
ApplicationIdentifier ClassApplicationIdentifier Members
Overload List
Base Implementation in Equals(Object)