Parameters
- fileName
- Specifies a file name in the demo directory to recall demo files. The file can be an HTML file (with the
.HTMextension), a setup file (with the .SETX or .SET extension), or a recording file (with the .SDF extension).
This method allows a setup file, a recording, and optionally a description of the setup to be recalled in a single operation. All files must reside in the same directory and have the same base name. For example, when the setup file is called "sample.setx", then the recording file must be called "sample.sdf" and the description file called "sample.htm".
The recording is recalled first, followed by the setup file and finally the description file. The description file, when present, is displayed in a separate browser window.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)