Keysight 89600 VSA .NET API
AverageStyle Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : AverageStyle Enumeration


Glossary Item Box

Specifies the type of averaging to be performed by the measurement.

Syntax

Visual Basic (Declaration) 
Public Enum AverageStyle 
   Inherits System.Enum
C# 
public enum AverageStyle : System.Enum 
C++/CLI 
public enum class AverageStyle : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
ContinuousPeakHoldSpecifies Continuous Peak-hold averaging.—
OffSpecifies no averaging.—
PeakHoldSpecifies Peak-hold averaging.—
RmsSpecifies RMS (Video) averaging.—
RmsExponentialSpecifies RMS (Video) exponential averaging.—
TimeSpecifies Time averaging.—
TimeExponentialSpecifies Time Exponential averaging.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also