Keysight 89600 VSA .NET API
Remove Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > CalibrationFileCollection Class : Remove Method


item
CalibrationFile to remove from the collection

Glossary Item Box

Removes the indicated CalibrationFile from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Remove( _
   ByVal item As CalibrationFile _
) As Boolean
C# 
public abstract bool Remove( 
   CalibrationFile item
)
C++/CLI 
public:
abstract bool Remove( 
   CalibrationFile^ item
) 

Parameters

item
CalibrationFile to remove from the collection

Return Value

True, if the CalibrationFile was removed from the collection.

Remarks

Note the first element in the collection cannot be removed because it is the primary CalibrationFile.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also