Keysight 89600 VSA .NET API
RemoveAt Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > CalibrationFileCollection Class : RemoveAt Method


index
Zero-based index of user to remove from the collection

Glossary Item Box

Removes the CalibrationFile at the indicated index from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function RemoveAt( _
   ByVal index As Integer _
) As Boolean
C# 
public abstract bool RemoveAt( 
   int index
)
C++/CLI 
public:
abstract bool RemoveAt( 
   int index
) 

Parameters

index
Zero-based index of user to remove from the collection

Return Value

True, if the CalibrationFile was removed from the collection.

Remarks

Note the first element in the collection cannot be removed because it is the primary CalibrationFile.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also