Keysight 89600 VSA .NET API
Equals Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > ChannelId Structure : Equals Method


Glossary Item Box

Determines whether the specified object is equal to the current ChannelId instance. (Overrides System.ValueType.Equals(System.Object).)

Overload List

OverloadDescription
Equals(Object)Determines whether the specified object is equal to the current ChannelId instance. (Overrides System.ValueType.Equals(System.Object).)  
Equals(ChannelId)Determines whether the specified ChannelId is equal to the current ChannelId instance.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also

Reference

ChannelId Structure
ChannelId Members
Base Implementation in Equals