| Overload | Description |
|---|---|
| ChannelId Constructor(Int32) | Initializes a new instance of the ChannelId struct that contains the specified channel number and a group number of 1. |
| ChannelId Constructor(Int32,Int32) | Initializes a new instance of the ChannelId struct that contains the specified values. |
| ChannelId Constructor(String) | Initializes a new instance of the ChannelId struct based upon a string that contains the specified values. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)