Keysight 89600 VSA .NET API
CreateOptions Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : CreateOptions Enumeration


Glossary Item Box

This enumeration is used to define specific VSA application creation options.

Syntax

Visual Basic (Declaration) 
Public Enum CreateOptions 
   Inherits System.Enum
C# 
public enum CreateOptions : System.Enum 
C++/CLI 
public enum class CreateOptions : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
InProcessCreate an in-process application.18.50
NoneUse the current setting for Utilities > Startup Preferences > Programmatic Startup.—
Use32BitCreate a 32-bit application even if 64-bit application is installed on the host.—
Use64BitCreate a 64-bit application.15.00
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

The ApplicationFactory.Create uses an argument of this type to specify non-default application creation options.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 14.00

See Also