Keysight 89600 VSA .NET API
Remove Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > CustomStepCollection Class : Remove Method


item
ICustomStep to remove from the collection

Glossary Item Box

Remove a ICustomStep from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Remove( _
   ByVal item As ICustomStep _
) As Boolean
C# 
public abstract bool Remove( 
   ICustomStep item
)
C++/CLI 
public:
abstract bool Remove( 
   ICustomStep^ item
) 

Parameters

item
ICustomStep to remove from the collection

Return Value

True, if the ICustomStep was removed from the collection.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also