Keysight 89600 VSA .NET API
CustomStepExecutingEventArgs Class Members
See Also  Properties 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : CustomStepExecutingEventArgs Class

Glossary Item Box

The following tables list the members exposed by CustomStepExecutingEventArgs.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorCustomStepExecutingEventArgs ConstructorOverloaded.   —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyIsRecomputingGets or sets a value indicating whether the step is recomputing.  —
Public PropertyStateGets the measurement state.  —
Public PropertyStatusCodeGets or sets a value indicating the success result of the step.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also