Keysight 89600 VSA .NET API
DataSource Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : DataSource Enumeration


Glossary Item Box

Specifies whether the data for the measurement is from measurement hardware or a recording.

Syntax

Visual Basic (Declaration) 
Public Enum DataSource 
   Inherits System.Enum
C# 
public enum DataSource : System.Enum 
C++/CLI 
public enum class DataSource : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
HardwareSpecifies input data is from measurement Hardware.—
RecordingSpecifies input data is from a Recording.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also