Keysight 89600 VSA .NET API
DataSourceValueToUse Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : DataSourceValueToUse Enumeration


Glossary Item Box

Specifies whether the data for the measurement is from measurement hardware or a recording.

Syntax

Visual Basic (Declaration) 
Public Enum DataSourceValueToUse 
   Inherits System.Enum
C# 
public enum DataSourceValueToUse : System.Enum 
C++/CLI 
public enum class DataSourceValueToUse : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FromCurrentStatePreserves current measurement's input data source.—
FromSetupFileUses input data source specified by the setup file.—
HardwareSpecifies input data is from measurement Hardware.—
RecordingSpecifies input data is from a Recording.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also